AXIS#.MOTOR.VOLTMIN

Description

This parameter configures the drive for the induction motor's minimum voltage at standstill. It is given as a percentage (%) of the motor’s rated voltage. AXIS#.MOTOR.VOLTMIN is used to calculate the constant volts per Hertz characteristics of the drive and motor and should be set to a value that generates a current of about 40% of the rated current at standstill.

Context

For more information see Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

%

Range

0 to 100

Default Value

2
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
AXIS1.MOTOR.VOLTMIN

500bh

07h

Unsigned16

-

-

Read/Write

No

AXIS2.MOTOR.VOLTMIN

510bh

07h

Unsigned16

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.MOTOR.VOLTMIN

6225

1851

Unsigned16

Read/Write

-

AXIS2.MOTOR.VOLTMIN

71761

1185

Unsigned16

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MOTOR.VOLTMIN

6225

Unsigned16

Read/Write

-